AXIS#.HOME.P

Description

AXIS#.HOME.P is the position given to the home point once it is found.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Rotary: counts, rad, deg, custom units, 16-bit counts

See Position Units for details.

Range

Depends on units. See Position Range for details.

Default Value

0

Data Type

Float

See Also

AXIS#.HOME.MODE
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
AXIS1.HOME.P

5008h

0fh

Signed32

Position

-

Read/Write

No

AXIS2.HOME.P

5108h

0fh

Signed32

Position

-

Read/Write

No

AXIS1.HOME.P

607ch

00h

Signed32

Position

-

Read/Write

No

AXIS2.HOME.P

687ch

00h

Signed32

Position

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.HOME.P

6109

17DD

Signed32

Read/Write

Position

AXIS2.HOME.P

71645

117D

Signed32

Read/Write

Position

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.HOME.P

6109

Signed32

Read/Write

Position

Related Topics

Homing